PRODUCT LIST
AC Power
Delta UPS Solutions - Industry-leading energy efficient power solutionsWith its wide range of Uninterruptible Power Supplies (UPS), Delta offers a competitive edge to businesses in need of first-rate power solutions. Delta UPSs are designed to ensure that companies can protect their mission critical applications by maintaining a steady flow of energy under adverse circumstances. An uninterruptible power supply is an electrical apparatus designed to furnish emergency power even when other sources of input power fail, and they are indispensable tools within a huge number of unrelated industries. These devices differ from a standby generator or an auxiliary or emergency power system in that in the event of a disruption to input power, a UPS will provide near-instantaneous protection for mission critical applications in the form of energy stored in batteries.
The high cost of electricity is not a factor that businesses can afford to ignore when considering their overhead. Every company, no matter how large or how small, must monitor its power use in order to avoid consuming too much. Delta UPSs are known for efficiency and for saving not just energy, but money that would be wasted by less advanced devices that require too much power.
The growth of a business should never be at risk of limitation or delay due to avoidable technical restrictions of existing power hardware. To help companies prepare for increasing success, Delta engineers flexible, scalable systems that are built to be easy to expand as needed, to accommodate greater demands for power protection.
The award-winning UPSs designed by Delta act as advanced power managers, ensuring the availability of an uninterrupted power supply to protect hardware and mission critical applications. High-quality UPSs function as an essential safeguard against many potential energy issues, including voltage surges and spikes, voltage sags, total power failure, and frequency differences. By making sure that their systems are set up to retain access to a stable power supply, even during failure events, companies can greatly reduce their costs while continuing to keep operations running smoothly.
The Delta line of uninterruptible power supply units includes superb options trusted by leading organizations across a wide array of industries, from financial institutions to medical centers. Small business owners also look to Delta for power solutions that keep their vital equipment running no matter what happens. The Agilon UPS family provides off-line UPSs up to 1500VA for personal computers, peripherals, and home appliances. Devices in the Amplon UPS family offer single-phase online UPSs with power ratings up to 12 kVA for servers and networking equipment. In the Ultron UPS family, three-phase online UPSs have power ratings of up to 4000 kVA, perfect for data centers, industrial facilities, and more. Three-Phase online modular uninterruptible power supply systems from the Modulon UPS family offer scalability and redundancy in a single frame, with up to 480 kVA. Delta’s UPSs are some of the most advanced in the industry, renowned for their innovation, reliability, and efficiency.
Delta also offers a large selection of accessories and monitoring software to complete and complement its UPS power solutions, ensuring compatibility among various components in an installation.
Product Family |
Power |
Topology |
Applications |
Agilon |
Up to 1.5kVA |
Single-Phase UPS |
PC and Peripherals |
Amplon |
Up to 10kVA |
Single-Phase UPS |
Server and Network Equipment |
Ultron |
Up to 500kVA |
Three-Phase |
Datacenter and Industrial Equipment |
Modulon |
Up to 200kVA |
Three-Phase modular On-Line UPS |
Modular Unit expansion and Redundant power supply can be achieved within a single rack |
Delta UPS systems feature the following:
- Leading AC-AC Efficiency
- Fully redundant and configuration design
- High input and output power factors
- Low iTHD
- Easily expandable without requiring additional hardware
견적의뢰 |