• Delta Telecom Power Solutions
  • Site Monitoring and Control System (SMCS) - Optimizing energy efficiency

    The SMCS includes an automatic input bypass functionality that connects rectifiers to mains power if the quality of the power supply is sufficient. Advanced generator management and monitoring features, and allowing a DC system to operate directly using AC power, are further examples of how the SMCS not only secures reliable power supply in all regions but also ensures optimal energy efficiency.

    The SMCS is designed to condition low-quality AC power, improve the availability of AC, and protect equipment from voltage variations and fluctuations. In addition, the SMCS acts as an interface between AC mains power, the diesel generator and the power plant in order to maximize the use of AC mains and battery power, and to minimize the operation of the diesel generator. The efficiency of the SMCS can be further improved by adding renewable power sources to the system.

    Read more about Site Monitoring and Controlling system from SolutionE -minisite: