• Delta Telecom Power Solutions
  • OutD cooling - Cooling power wherever you need it

    Cooling plays a critical role in site energy consumption: it requires roughly as much energy as the actual telecom equipment. The advanced climate management features of Delta’s OutD solutions reduce the amount of energy needed for cooling by up to 80%.

    Our new OutD solution features a separate battery cabinet, which is cooled more effectively than the rest of the cabinet, using thermoelectric cooling. While other system equipment may function perfectly at much higher temperatures, battery cooling is extremely important, because a 10 °C rise in temperature in the battery cabinet halves the lifetime of a battery. We use energy for cooling only when necessary.


    Read more about Delta's solutions for cooling: 

    Explore SolutionE: