PRODUCT LIST

  • Delta Telecom Power Solutions
  • SSW Series static switch

    Introduction

    The Delta SSW Series static switch provides uninterruptible AC power by acting as an electronic switch between the AC mains and the Delta API 1500A series modular inverters. The two standard static switch modules are designed for 7.5 kVA and 30 kVA output, respectively.

    The static switch ensures that the system performs without interruptions and that the modular inverters are synchronized to the AC mains. The optimized architecture of our solution provides energy savings of up to 5%. In addition, when the static switch is configured to offline mode, in which the AC utility is connected to the equipment directly, energy savings can reach up to 14%.

    top